FB#.POLES

Description

FB#.POLES sets the number of individual poles in a resolver feedback deviceClosedA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position. This variable is used for the commutation function, as well as for velocity feedback scaling, and represents the number of individual poles (not pole pairs). The division value of motor poles (AXIS#.MOTOR.POLES ) and feedback poles (FB#.POLES) must be an integer when moving drive to enable, otherwise a fault is issued.

Context

See Feedback Devices.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

2 to 510

Default Value

2

Data Type

Integer

See Also

AXIS#.MOTOR.POLES

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen FB1.POLES 0x3500 0x3 UINT - - RW False
FB2.POLES 0x3501 0x3 UINT - - RW False
FB3.POLES 0x3502 0x3 UINT - - RW False
FB4.POLES 0x3503 0x3 UINT - - RW False
FB5.POLES 0x3504 0x3 UINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen